Step Jogging Tool URCap

JogTool-1.0.3.urcap (228.8 KB)

Hi, as the whole world being overwhelmed by PolyScope X, there are still some users utilizing PolyScope 5 in real application, the build-in Move UI only permit me to do a continuous jogging, and here is a complementary Jogging tool with more options of Step Jogging with 0.5/1.0/5.0/.. mm per click. Hope it will be helpful to your work and welcome for any feedback.

* it can switch displayed language according to PolyScope language, currently it can only accommodate EN / TW / CN / JP / ES / DE / FR / KR, thanks to my global team help🎇

1 Like

Could be useful, thanks for sharing! If you didn’t know, you CAN do this with the built-in UI. Just click any of the value boxes

Then select Tool (or any other Feature) and hit the “+” or “-” button by the appropriate direction. You then type whatever distance you need and hit OK. The robot will then jog by that set amount.

If you had to do this a lot, it could get tedious, which is where your CAP could still be useful.

1 Like

Yeah, the built-in UI indeed provides a possibility to step moving along with TCP i believe that’s why till recent nobody raise hand on this point: i counted that it needs to click 5 times on TP to perform one step move; for the use case i need to jog along with a non-tool feature, as values are not zero in the boxes, then i have to do math+5clicks :rofl:

With this urcap, i just click-move, click-move, which is the core part of it :wink:

1 Like

Good idea! I may use it.
I think 0.1 instead of 0.5 mm step may be more useful.

Oh yes this part hasn’t been fully elaborated, the tool provides 0.1mm step as part of a full list in below snapshoot :wink: @pgy

1 Like