How to backup the .urcontrol folder

Hi,
Today I met a problem.I can’t use my ur-5.I press the switch and the system will automatically shut down after a while.So I think the system disk is broken.So I use the robot image software to make a new system disk.
image
So how do I get these files out of the picture especially ‘.urcontrol’.I want the DH parameters of the robot, which is important to me.
How can I get the ‘.urcontrol’ and Write this into the new system disk?
Thank you.

If your UR robot is connected to the local network with Ethernet you can mount remote directory on your local computer with sshfs command (you run this command on local computer):
sshfs root@<IP_ADDRESS_OF_UR_ROBOT>:<DIR_ON_UR> <LOCAL_DIR>
for example:
sshfs root@192.168.1.50:/root ~/remoteURDir

It works great on Linux. Then it is easy to upload/download files from UR.

Default password for root is: easybot

@anon73581494 check this out… we’re releasing some of our cloud capabilities to the community. No cost backups with no extra hardware required.