URCap installation problems

Hello,
I have a UR10 CB-Series robot running PolyScope 3.15.2 (URSoftware 3.15.2.106179).

I am trying to integrate a Roboception rc_visard 160C using the Roboception URCap.

The current rc_urcap 3.2.0 installs, but after reboot PolyScope reports:

URCap requires package ‘m.roboception.rc_urcap [472] (R 472.1)’ which is not available.

What can i do?

Contact the CAP developer with this error. They should be able to provide the dependency or at least point you in the right direction.