Dear all,
I recently upgraded our UR10 to the latest Polyscope version for use with a Robotiq force sensor.
Since the upgrade, it has become impossible to install URCaps (so far, I’ve only tried 2 from Robotiq). Upon reboot after URCap installation, the teach panel gets stuck on the boot screen at 100%. After that, the only remedy seems to be to flash a new OS on the CF card, but this causes the same issue (robot-specific files copied according to manual).
Once, I also had the issue after flashing the OS. This problem seems to have gone away by not copying ur-serial and flightreports to the CF card.
Am I missing something here?
OS image: Controller_USB-CB3.1-3.15.4-build10.6.291.img
Robot model: CB3UR10
The only odd thing that I was able to see was this entry in /var/log/boot.log:
fail: /etc/service/urcontrol: runsv not running
Best,
Nikita