Hi Everybody,
I’ll start by saying I’m a new user.
I’m working with a UR5e , equipped with a camera on it. The camera is pretty heavy and the calculated payload is close to the limit.
I’m sending through a socket 3 positions (looks like “p[0,0,0,0,0,0]”). The last position I’ve sent almost ended in a crash, so I pressed the Emergency push button.
From that moment, although the values of the - Payload, TCP, Center of Gravity - didn’t change, when I press the manually-move little black button, the robot is moving up like something has changed in the configurations.
- This movement didn’t occure after I configured the Payload, TCP, Center of Gravity, and I could pressed the manually-move little black button and the robot was waiting there, soft as butter.
- I’m moving the robot in a small area, without stretching the joints, and without challenging the robot (for now at least).
- Because the payload is close to limit, I’m moving the robot slowly.
- For the second question:
I’ve put the robot in some position in the area, and pinned that point as a “movej” target. Then from the “Run” screen I thicked the “show waypoints” so I could understand for which measuring units of the points, the robot is expecting Found out its Meters, after trying to send points in mm, as all the user interfaces are.) The only axis that was different between the waypoint pinned in mm, to the waypoint in Meter from the “Run” screen, was Z axis. one of them was a negative value (the pinned point), and one of them was a positive value(Run screen). I’ve attached a snip.
So after telling you all that, I have two questions.
- Is the robot behavior after emergency stop, as described, is normal?
- Why the difference between the two showing methods of the same point?
Thanks,
Elad.