I’m using the RTDE interface to update the speed_slider_fraction value, and it works in most cases. If I try to update the value to 0 it doesn’t work on simulator version 3.14 (CB series), speed slider value only goes down to 2%. But on simulator version 5.9 I was able to update the speed slider value to 0% without any issues.
Is this a limitation on CB series robots?
Thanks.