You don’t want them to be using the pendant, but it will be the user proactively resuming the program? Would a push button connected to a digital input configured to play the program be acceptable? This can be configured under the IO Setup menu of the installation tab.