I need to be able to WRITE general purpose registers via RTDE.
Unfortunately, up to now, i could not find a way to WRITE (and read) those general purpose registers since the only commands that are available deal with integer and float registers.
Has someone faced this problem?
Has someone already wrote on BIT registers via RTDE?
Could someone give me some hints about a possible solution? Do I have to implement a RTDE client to write these general purpose (bit) registers?
I am working on this issue from some time and i cannot find a way out
I have a question: my goal is to WRITE_INPUT_BIT_REGISTER but you have used a command to write_output_bit_registers. how could i WRITE these input bit registers since no command is available on the ur scripts ?
my goal is to write the input bit register via RTDE.
Just so I understand, you are trying to have your PC code write to the robot’s input bit registers? If so, then yes you can do this via RTDE. Your XML file would look something like this:
In my case I chose register 70, but you can choose any number from 64 to 127 (registers 0 to 63 are reserved for fieldbus/PLC’s and are therefore unavailable). From there you should be able to follow the examples in those guides for sending a new value; you can either use an integer 0/1 or a boolean True/False to change them.
On the other hand, if you are trying to have your PC code write to the robot’s OUTPUT bit registers (or any for that matter), that will not be possible.
So you are working with python, trying to write into the boolean input registers over RTDE correct?
Have you had any success with RTDE communication at all yet? What errors are you seeing?
Expanding on @krmi’s example above, the below config and python sample pair is adapted from example_control_loop.py that’s included with the RTDE library download from the support site. It will both read and write input bit reg 70, and toggle the value between true and false each time you run it. Hopefully this gives a clear example of how to interact with this register through RTDE. It addresses the RTDE at localhost, so assumes you’re running this script on the robot or in the same environment as URSIM.
save as "example_boolreg_configuration.xml"
<?xml version="1.0"?>
<rtde_config>
<recipe key="outputs">
<field name="input_bit_register_70" type="BOOL"/>
</recipe>
<recipe key="inputs">
<field name="input_bit_register_70" type="BOOL"/>
</recipe>
</rtde_config>
#!/usr/bin/env python
import sys
sys.path.append('..')
import logging
import time
import rtde.rtde as rtde
import rtde.rtde_config as rtde_config
logging.basicConfig(level=logging.INFO)
ROBOT_HOST = 'localhost'
ROBOT_PORT = 30004
config_filename = 'example_boolreg_configuration.xml'
keep_running = True
logging.getLogger().setLevel(logging.INFO)
conf = rtde_config.ConfigFile(config_filename)
output_names, output_types = conf.get_recipe('outputs')
input_names, input_types = conf.get_recipe('inputs')
con = rtde.RTDE(ROBOT_HOST, ROBOT_PORT)
con.connect()
# get controller version
con.get_controller_version()
# setup recipes
con.send_output_setup(output_names, output_types)
inputs = con.send_input_setup(input_names, input_types)
#start data synchronization
if not con.send_start():
sys.exit()
#inputs.standard_digital_output_mask = 1
print("running now")
# control loop
while keep_running:
# receive the current state
outputs = con.receive()
if outputs is None:
break;
reg_value = outputs.input_bit_register_70
print("reg70: "+str(reg_value))
inputs.input_bit_register_70 = not reg_value
con.send(inputs)
break
con.send_pause()
con.disconnect()
In this week i have tried working with this and i have encountered the following issue:
As proposed by @ajp , i have set my input/output registers with a “free” number that can be selected each time in a different way
My goal is to associate to the values of those registers some actions (like to get the TCP value after that a push button has been pressed)
in order to perform this association, i have tried adding to my .xml file these ne inputs/outputs. For example, in the output section, i have added a new line of the following form
field name=“regOutBit1” type=“BOOL”/>
where
x = 70
regOutBit1= ‘input_bit_register_’+str(x)
setattr(inputs,reg,True)
This mechanism seems not to work since i get the following error:
File “/home/ur/Desktop/boolFinale_v5/rtde/serialize.py”, line 193, in unpack_recipe
raise ValueError('Unknown data type: ’ + i)
ValueError: Unknown data type: NOT_FOUND
I have tried having a look at the serialize.py and at the other .py files but i could not figure out how to proceed.
Sorry if that was not clear, you can’t do that in the XML file. You need to hard code the registers in there. So you’d need to include every register that the user could possibly choose to use:
Hi!
I got what you sad, maybe i was not clear about my doubt.
I have hard coded every needed register inside the .xml and this is fine to me.
my goal is to let the user be able to choose at startup which register he wants to use: for example, when i run python my code
python3.8 test.py 101 102 103
since it is possible to do it thanks to your previous answer, i am able to set these registers via
x = 70
regOutBit1= ‘input_bit_register_’+str(x)
setattr(inputs,reg,True)
i have set these bindings in my program and then, i have followed the following idea:
since i have set regOutBit in the previous way, then i am able to assess the state of this register by outputs.regOutbit (due to the fact that RegOutBit in the reality is input_bit_register_x)
Unfortunately, while i try to assess these registers, for example with the following syntax
if output.regOutBit == 1:
do something
i get the following error
File “/home/ur/Desktop/boolFinale_v5/rtde/serialize.py”, line 193, in unpack_recipe
raise ValueError('Unknown data type: ’ + i)
ValueError: Unknown data type: NOT_FOUND
i cannot figure this error out since i am using RegOutBit = output_bit_register_x and in the .xml i have hard coded all the needed registers.
have i been a bit more clear about my issue?
I am sorry if my English is not clear enough
Back to the topic of setting up your XML config, I thought you would be receiving the registers the user wants to use via RTDE not via command line.
As you’re getting this from the arguments, you could actually build your XML config file in python and write it to file before using it to set up your RTDE connection. (this may be overcomplicating things, feel free to skip over this).
#!/usr/bin/env python
import sys
sys.path.append('..')
import logging
import time
import rtde.rtde as rtde
import rtde.rtde_config as rtde_config
#BUILD XML CONFIG BASED ON COMMAND LINE ARGS
arg = str(sys.argv[1])
xml1 = """<?xml version="1.0"?>
<rtde_config>
<recipe key="outputs">
<field name="input_bit_register_"""
xml2 = """" type="BOOL"/>
</recipe>
<recipe key="inputs">
<field name="input_bit_register_"""
xml3 = """" type="BOOL"/>
</recipe>
</rtde_config>
"""
xml = xml1+arg+xml2+arg+xml3
config_filename = 'example_boolreg_configuration.xml'
file1 = open(config_filename, "w")
file1.write(xml)
file1.close()
logging.basicConfig(level=logging.INFO)
ROBOT_HOST = 'localhost'
ROBOT_PORT = 30004
keep_running = True
logging.getLogger().setLevel(logging.INFO)
conf = rtde_config.ConfigFile(config_filename)
output_names, output_types = conf.get_recipe('outputs')
input_names, input_types = conf.get_recipe('inputs')
con = rtde.RTDE(ROBOT_HOST, ROBOT_PORT)
con.connect()
# get controller version
con.get_controller_version()
# setup recipes
con.send_output_setup(output_names, output_types)
inputs = con.send_input_setup(input_names, input_types)
#start data synchronization
if not con.send_start():
sys.exit()
#inputs.standard_digital_output_mask = 1
print("running now")
# control loop
while keep_running:
# receive the current state
outputs = con.receive()
if outputs is None:
break;
reg = 'input_bit_register_'+arg
reg_value = getattr(outputs,reg)
setattr(inputs,reg,not reg_value)
print(reg+": "+str(reg_value))
con.send(inputs)
break
con.send_pause()
con.disconnect()
I am facing a similar problem with the RTDE interface.
I have seen that the input bit registers 0to63 are reserved for the plc.
is there a way in which i am able to write on these registers (via rtde or else) so that then my plc is able to see a change in these registers and as a consequence perform a given action?
Hi @anon84921795 What you propose is NOT possible. Once you enable the fieldbus interface (profinet or ethernetip) the ‘driver’ within UR control will be writing to these reserved input bit registers (0-63) as it is expecting to get data from the PLC’s scanner. Anything you write via RTDE will get over-written by the PLC interface.
You should be using output registers of the robot to signal information back to the PLC.
Hi all! I am currently working with a UR10e and I am experiencing trouble passing a boolean through the input bit registers. I am following exactly the scripts from this post. On my teach pendant in Polyscope I am simply running:
var_1 = read_input_boolean_register(70)
sync()
When first running the Python script I get a C207A0: Fieldbus input disconnected error. I have disabled all fieldbus/Profinet/ethernet options in the installation tab.
When first running my Polyscope program I get the following error in my Python script: ValueError: An input parameter is already in use.
Is there anyone who could help me? All posts I can find on the C207A0 advise to turn of Profinet or ethernet/IP settings which I have done already.