Hi there, is it possible to read/write general purpose registers through TCP/IP communication not using RTDE? I need to write and read data from registers, and I can’t find the way to do that using the Real-time interface through port 30003. Also, I am having many difficulties to do that via RTDE because I am not using Python or C++, I am using C# instead and it is a bit complicated to make it work.
Please I would highly appreciate any hint or help you can provide. Thank you!
If you’ve got budget for extra libraries, UnderAutomation has a C# library for communicating with UR bots, including RTDE. It has a free trial option, so you can test it out to see if it serves your needs.
using UnderAutomation.UniversalRobots;
using UnderAutomation.UniversalRobots.Common;
using UnderAutomation.UniversalRobots.Rtde;
using UnderAutomation.UniversalRobots.Rtde.Internal;
class Rtde
{
static void Main(string[] args)
{
var robot = new UR();
var param = new ConnectParameters("192.168.0.1");
// Enable RTDE
param.Rtde.Enable = true;
// Exchange data at 500Hz
param.Rtde.Frequency = 500;
// Select data you want to write in robot controller
param.Rtde.InputSetup.Add(RtdeInputData.StandardAnalogOutput0);
param.Rtde.InputSetup.Add(RtdeInputData.InputIntRegisters, 0);
// Select data you want the robot to send
param.Rtde.OutputSetup.Add(RtdeOutputData.ActualTcpPose);
param.Rtde.OutputSetup.Add(RtdeOutputData.ToolOutputVoltage);
param.Rtde.OutputSetup.Add(RtdeOutputData.OutputDoubleRegisters, 10);
// Connect to robot
robot.Connect(param);
// Be notified at 500Hz when data is received
robot.Rtde.OutputDataReceived += Rtde_OutputDataReceived;
// Get last received data in cache
Pose actualTcpPose = robot.Rtde.OutputDataValues.ActualTcpPose;
int toolOutputVoltage = robot.Rtde.OutputDataValues.ToolOutputVoltage;
double outputDoubleRegisters10 = robot.Rtde.OutputDataValues.OutputDoubleRegisters.X10;
// Write input values in robot
var inputValues = new RtdeInputValues();
inputValues.StandardAnalogOutput0 = 0.2;
inputValues.InputIntRegisters.X0 = 12;
robot.Rtde.WriteInputs(inputValues);
// Disconnect every interfaces (Primary Interface, Dashboard, RTDE, ...)
robot.Disconnect();
}
private static void Rtde_OutputDataReceived(object sender, RtdeDataPackageEventArgs e)
{
// Get frequency of received message (OutputSetup contains Timestamp by default)
var realMessageFrequency = e.MeasuredFrequency;
// Get the value of the data you have selected in the setup
Pose actualTcpPose = e.OutputDataValues.ActualTcpPose;
int toolOutputVoltage = e.OutputDataValues.ToolOutputVoltage;
double outputDoubleRegisters10 = e.OutputDataValues.OutputDoubleRegisters.X10;
// Write inputs at 500Hz
var inputValues = new RtdeInputValues();
inputValues.StandardAnalogOutput0 = 0.5;
inputValues.InputIntRegisters.X0 = -10;
(sender as RtdeClientBase)?.WriteInputs(inputValues);
}
}