I’ve reviewed the robot’s limits, and it seems the maximum speed limit is set at 1500 mm/s. I know that joint rotation is measured in rad/s, but I’d like to know what the maximum speed limit is for rotation.
When moving the robot arm to a position using Movel, the instantaneous rotational speed of the joints sometimes becomes excessively high, causing an error. How should the robot be operated to prevent this?
If you’re moving at those speeds, you have to make sure your TCP, payload, CoG and preferably inertia settings are all set up correct. And make sure you’re running the latest Polyscope (and try out Motion Version 2). That might help you with your stops.
If you’re actually using a UR5 CB2/3 (and not a UR5e), you will not be able to do much and might have to lower your speed settings.
But you can set up max rotational speed for each joint in the safety settings. That might help you.