How can I run an urscript in my urcap directly, after the robot booted?
generateScript in Installation Node is executed after program is running.
I want to run this thread after robot is booting. thread myThread(): while (True): // Do some stuff end end run Timer_Thread()
Hi @bernd.heinzmann,
You can send it to the controller on port 30001. The operator of the robot will be able to stop that program by the stop/pause button or starting another program. I have a snippet from a bash script for reference:
printf "def prog_test():\n%s\nend\n" "$(cat $1)" | nc localhost 30001
So your script should be incapsulated in a function definition. Else the controller will interpret one line at a time.
Ebbe