Robot mounting and Angle

Summary

I would love to be able to specify a specifc Mounting angle on un the installation menu. I propuse that the angle are actually number input fields where one can write the specific angle one want.

Provide a one-line description of the feature
Specify a specific angle in the mounting menu.

Why is it needed?

The mounting holes on the robot are at a 22.5 degree difrance however it is almost imposible to actually get the 22.5 angle…

1 Like