Good morning together,
I´m facing an issue with the IP-Address of my UR10e.
The UR is connected to a Siemens PLC and Siemens HMI.
The IP Address are:
PLC: 192.168.100.1
HMI: 192.168.100.2
UR: 192.168.100.3
When I set the adress via Siemens TIA v15.1 I can communicate between the Robot and my PLC. BUT!!!
When i take a look at the Robot Panel it shows the IP adress of 192.168.100.3 NOT at its IP Address. It says the Standart Gateway Address is “192.168.100.3”…
When i try to change it “manually” at the Robot Panel:
and then I press “Übernehmen” (Apply changes), again all values will be set to 0.0.0.0 and at the Standart Gateway it will put the address to “192.168.100.3”.
Does anyone has an idea why it is like that?
For now its working, but later we want to connect the Robot to the Plant network (for that we use the gateway 192.168.100.80)
Kind regards from Luxemburg