Polyscope X 10.12 - Ethernet/IP

Does anyone tried to communicate using Ethernet/IP on Polyscope x 10.12 to PLC? I don’t know why the polyscope X 10.12 intermittently gets connected then no scanner (on a loop) with keyence KV-7500 and KV-XLE02. I use the Universal Robot EDS file and tried to increase the RPI from 10ms - 50ms but still got this trouble.

PS. I also tried this set-up on Polyscope 5 and didn’t encounter this issue.

@v51 It does happen with some PLC vendors and we’re trying to pinpoint the root cause.
There is a feature to record E/IP communication in 10.13 ( Release Notes 10.13.X )
Could you update, enable “network diagnostics”, try to connect from PLC and take support file?
PM me with support file.

I’m on 10.14 and trying to communicate with TwinCat 3 TF6281 EIP Master, and even after setting up everything correctly, the Robot Controller refuses to connect. Tried to enable network diagnostics, restart service, etc, but the support file doesn’t contain the .pcap file somehow. Is there any EDS file for Polyscope X? Or should it work with basic settings?