Output signal when the UR Robot enters in Protection Stop or Emergency Stop

Hi,

I would like to now if its there a way to make the robot alert via an output signal when it enters an emergency stop, for example , when it hits something, it stop automatically, but i would want to output a signal to a speaker alarm, so the person in charge of the operation of the robot hears this protection stop.

Best Regards,
César Correa.

There are a few ways you can accomplish this task. For example you could access the internal modbus server on the controller and monitor the isProtectiveStop isEmergencyStop addresses, more info:

https://www.universal-robots.com/how-tos-and-faqs/how-to/ur-how-tos/modbus-register-and-digital-io-19252/

https://www.universal-robots.com/how-tos-and-faqs/how-to/ur-how-tos/modbus-server-16377/

You could do similar approach using the client interfaces:

https://www.universal-robots.com/how-tos-and-faqs/how-to/ur-how-tos/overview-of-client-interfaces-21744/

Or through some IO setup on polyscope as well:

Thanks, this is exactly what I needed

Do you just choose any Configurable Output and set it to Not Reduced Mode?

Hi!

Will the Not Reduced Mode state change when the robot goes into Safe Guard mode?

Thanks.