Multiple ursims

Hi,
Im working on simulating a robotic cell with multiple robots. I connected four pc’s to a network, three of the are running two VM’s each with ur sim. The fourth one is the host and running RoboDK.
Im having connection issues with the VM’s. When pinging the VM’s from the computer they are running on the connection is good. When pinging the pc’s from the host computer the co nection is good as well. But when pinging the VM’s from the host the connection is terrible. Its that bad that I can’t connect to them via the cpp API which is running on the host.
Any ideas?
Thanks for your help,

1 Like