Dear Developers,
In my application I would like to completely hide TP from the operator, however I have the impression that the functions written in the robot software do not allow me to do this, so please help me how to do it.
My robot is CB3.
I divided the initialization into stages step by step and it turned out that as many as 5 steps I can not do / see without TP.
Help please, maybe I’m making a mistake somewhere

Initialization with TP
I press the turn on button on TP, I can see that the robot has started because the button is green.
I am waiting for the screen with UR main software on TP to appear allowing the robot to be initiated.
I see a red dot, the robot is turned off, I press the buttons one after the other to start the robot.
I can see that the robot’s status is Power On. I run the program.
I want to turn off the robot. I press the on button or select the appropriate function on the screen.
Initialization without TP.
I press the ON button connected to the ON socket in the robot’s cabinet.
I have no confirmation if the robot is powered because there is no electrical output with such a signal.
I do not know when the robot will initiate its control program because I do not have an electrical output that indicates it.
The robot’s status is sent only through communication ports without any additional device, I don’t know if the robot is in POWER OFF state.
I press the button, release the brakes to start the robot. Button attached to the appropriate DI with this functionality.
I use the button to start the program. Button attached to the appropriate DI with this functionality.
I want to turn off the robot, I press the OFF button connected to the OFF socket in the robot’s electrical cabinet.
Thanks in advance for your help.
Regards,
Michał