External Control URCapX fails to install on PolyScope X 74.23.218 (Manifest file missing)

Hello everyone,

I’m currently setting up a ROS 2 Jazzy environment with a UR7e robot (e-Series, manufactured recently – August 2025).
The robot is running PolyScope X version 74.23.218.

When I try to install the External Control URCap X (required for ROS 2 control) I get the following error message on the Teach Pendant:

Cannot install URCap

: Manifest file (META-INF/MANIFEST.MF) is missing

Steps I followed:

  1. Downloaded externalcontrol-0.1.0.urcapx from the official GitHub release page:
    https://github.com/UniversalRobots/Universal_Robots_ExternalControl_URCapX/releases

  2. Copied the file to a USB stick (root directory).

  3. Installed via Settings → System → URCaps → + (Add URCap).

  4. The error appears when i select the file (external-control-0.1.0.urcapx).

I double-checked the file name and integrity, but PolyScope still refuses to install it.
It looks like my robot expects a newer, signed URCapX package format for the 74.x firmware.

My questions:

  • Is there an updated version of the External Control URCap X compatible with PolyScope 74.x ?

  • If not yet released, is there any workaround (for example using RTDE directly with the ROS 2 driver)?

  • Should I request a signed URCap package from UR Support?

Any feedback or confirmation from users running PolyScope X 74 would be greatly appreciated! :folded_hands:

Thanks in advance for your help.

Hi Sabrina,

sorry for a very late reply, but I just stumbled upon this topic and wanted to still provide an answer for anyone else looking at this.

From the Screenshot it looks like you are trying to install a PolyScope X URCapX File onto a PolyScope 5 System. This can not work. You will need to download the PolyScope 5 External Control URCap with the Ending “.urcap”