I am using a UR7e with a CB5.6 controller running PolyScope X 10.11.
For my research setup (ROS2, External Control, Robotiq 2F-85, and third-party integrations), I have found the user experience and compatibility on PolyScope X significantly more difficult than on PolyScope 5. Many existing tutorials, URCaps, and community resources are still centered around PolyScope 5.
Is it officially supported to downgrade a CB5.6 robot from PolyScope X 10.11 to PolyScope 5.26 LTS?
If so, what is the recommended procedure, and are there any known limitations or risks?
Procedure would be to start with a fresh SD card and mount the image. Nothing else is needed. I would suggest keeping the X sd card to be able to easily swap back and forth. From what I can tell, there is nothing stopping you from flopping back and forth. the robot just updates firmware every time you power on. I would suggest doing backups before switching just in case though
Doesn’t even need to be an SD Card, USB Stick works fine as well (but might require playing around with UEFI boot order (can’t remember details as I do such things in autopilot mode)
I tried this yesterday *(with a usb drive 16gb) and just gave me an infinite boot load screen… the initial message when it turns on says it’s loading polyscope 5 and then sits on universal robots screen with the circle as if it’s loading… I waited about 45 mins because I know the first boot can take a while but eventually gave up. What was I doing wrong you think?
I also experienced such things but while playing around with Polyscope X Prereleases. I guess your Polyscope X was installed on the SD Card, not on the eMMC (you would know if you dont know what Im tslking about, you are fine).
I would contact your Distributor / Integrator to double check the warranty terms in case of a software change, because rather than just downgrading, you are changing the entire OS type of version.
In terms of ROS2, Polyscope X comes with that natively integrated and a REST Robot API that replaces the Dashboard Server, I would rather recomment to upgrade to Polyscope 10.14 rather than downgrading to Polyscope 5,
In any case, the procedure is as always: re-flash a SD card with whatever software you want to run. Notice that Polyscope X might take longer to boot through SD card than EMMC memory allocation.
Finally, as precaution regarding the warranty, I would keep Polyscope X original SD intact and use a new SD card for Polyscope 5.