Is ist possible to access members of an XMLRPC struct in URScript?
In our Use Case we have something like this:
{
"returnCode":0,
"returnValueType":"Pose",
"returnValue":{"x":-0.259182,"y":-0.443102,"z":0.643896,"rx":1.08664,"ry":2.64558,"rz":0.112022}
}
Now we would like to use the Pose in URScript.
Is there a way to do this?
short answer is no, urscript cannot handle lists of various types and therefore cannot handle a dictionary-like object.
however - there is one exception: poses. they can be transferred via xmlrpc with a dictionary-like object, but afaik only on their own. the format in order for urscript to interpret it as a pose is exactly as you have it:
{"x":-0.259182,"y":-0.443102,"z":0.643896,"rx":1.08664,"ry":2.64558,"rz":0.112022}
return that from the xmlrpc server and urscript reads it as a pose.
See here:
https://www.universal-robots.com/articles/ur/interface-communication/xml-rpc-communication/
the zip at the bottom has a python and cpp example that return poses via xmlrpc.
Thanks for the response 
Yes, we have used XMLRPC to provide poses. We hoped since this somehow magically works, that there is some way to also parse maps with different content.
But we will look for a different way