Speed slider can be controlled with doing the following.
Is “set” the urscript command?
Are there parameters other than “speed” that can be set.
Hi,
i don’t understand this either. It has something to do with the robot messages described in the attached xls file of the Secondary/Primary Interface. The doc above says it can only recieve URScript commands (which set speed does not count to) which isn’t the whole thing.
@jbm can you enlighten us? ![]()
@m.birkholz
There are no documented commands, beyond the “set speed” control command.