Does anyone know where these settings are stored on the controller? Like in the underlying Linux file system? Since the new version of Polyscope, these settings all come in disabled, and we use several of them for our systems, so it’d be nice to add this to the auto-configuring flashdrive we use to set them up. @bba
Eric,
I am checking with someone else.
Hi @eric.feldmann ,
Configuring the services to be open from the start (I assume it would be done by a magic file), will require admin login and enabling of magic files, as they are also disabled by default. This means someone would still have to (manually) use the polyscope GUI to do these things before an automated utility could be used.
Understood. I’d still like to know where the file is stored so I can remove as much human interaction as possible. I’d rather NOTHING work due to someone not running the magic file as opposed to just SOMETHING not working because they accidentally forgot to enable ONE of the services.