Is there any documentation that talks about file locations and how to get access to files without going through the magic file process ?
I see that there is an SSH server running. I can hit it but can’t find a username / password.
I would like to be able to SSH into my UR5 and place program and configuration files on the unit from a remote computer.
Is there a guide to where the program files go ? Configuration files ?
Any help is appreciated.
Thanks,
Mark
Hi Machollett
Program files and installation files reside in /programs folder. You can use username as root and pwd as easybot.
Thank you for the information.
The .urp .script and .txt files go in the /programs folder.
Do the .installation and .variables files also go in the /programs folder or are they stored in another location.
Thanks,
Mark
Installation files (including variables) are all stored in /programs/
All user accessible files should be stored here.
In current software (5.3, 3.9) all services in the robot is executed as root.