Magic Files for URControl files

Hi, I would like to use magic file to change the urcontrol file, is it allowed by the robot? How can i do it? I want to change the urcontrol file so for my project

Take a look at my post here. I used magic files to modify some of the system files.

But i want to change polyscope files, such as urcontrol.conf file

That’s…what the post details how to do. Polyscope is reading the contents of those files. If you change them in the linux backend, you change what Polyscope reads/boots with. If you can find the file you’re interested in changing via the terminal, then you can use the process outlined in that post to do so. Just replace one of the file paths I had used with the one you want. In fact, I was already modifying the .urcontrol file in that example

I made these mostly by either copying it from my simulator, or else copying it from the actual robot controller. Then I changed what I needed and wrote the cp command to write it back.

So copy the .urcontrol.conf, edit it with whatever text editor you want, save it to your flashdrive, and add/modify a line of the magic file to cp/path/on/URcontroller your/saved/path

Thank you so much and apologies for a very delayed response