The latest urmagic_screenshot.sh was pulled from the download library, extracted, and loaded on the root of a USB drive.
The USB drive was inserted in the pendant. The red “! USB !” warning sign will appear, indicating a screenshot is taken. The green “<- USB” sign appearing, indicating the screenshot is completed never appeared or flashed so fast I did not see it. The /screenshots directory was not created on the USB drive and no .png file was created. I left the USB plugged in for 5 min.
The instructions say to just extract the .zip to the root of the USB drive. I did this, and then inserted the USB drive into the pendant and nothing occurred.