Hi there,
I am new to the forum and the realm of robotics ![]()
I am working with a UR5 CB3 and I want to create a prototype for optical part inspection.
The task basically is:
- Pick items from a tray - rectangular shape, fixed positions of the parts
- Perform the inspection task in between, a software decides if the part is ok or not, and depending on that,
- Put the part in the “good” or the “bad” box, again, boxes with fixed positions where the parts should go.
Right now I am in the process of creating the robotic path and inspection sequence. I used the palleting wizard to create 3 pallets. One to pick and two to drop of.
At the pickup box and the good part box, it is critical that the parts are put there with a lower speed. However, I haven’t figured out how to change the speed of the palleting mode. I tried to change the waypoint speeds of the approach and the first pattern point, but it had no influence. The parts are literally hammered into those boxes.
I tried to add a Move command into the palletizing wizard, however it would not compute until I deleted the Move command again.
So far, the search in this forum and chat gpt could not help me with my issue.
So I am counting on you guys and gals here.
Thanks for your help,
Anton