Unknown Function: findmodel

Hey everyone,

I’m currently working with a UR3e and the Robotiq Wrist Camera, and I’m experiencing the same issues shown in this past forum post, following the same steps.

Link to the post: Unknown Function: findmodel

Has anyone managed to figure out what’s happening here?

Have you tried contacting Robotiq?
Are you also trying to send the whole program through one of the interfaces?
have you installed their URCap as this is most likely where the function gets defined?

I haven’t reached out to Robotiq yet. I’m currently attempting to send the program with the .script extension to the robot from my computer using a Python script. As for the URCap, I haven’t been able to install it yet.

Yeah that properly why then.
one of the things a URCap does is basically to define a bunch of functions in the top of any script file created through the teach pendant to give you new functionality.
while I have never used Robotiq I bet you will find the findmodel function you are looking here.

But this also means that you cant just use external programs like what you are doing now, and as the guy in the post did.
As these functions simply is not defined in the script file you create on you own pc.

What I would do is

  1. get the urcap installed
  2. create a random program on the teach pendant that does basically nothing
  3. save it
  4. transfer the created script file to a usb and then to your pc.
  5. open the file and copy paste all the functions that the urcap auto generates
  6. add something in the top of your python script that appends this to the start of your script file.

and do keep the URcap installed as the functions most likely calls a bunch of background processes (know as daemons). which you will remove by uninstalling the urcap.
Kind Regards

1 Like