Start_prog and stop_prog dosen't work anymore

Normally, I used two GPbi registers to pair them with the start_prog and stop_prog functions to remotely control the start and stop of the program via Ethernet_ip. In version 5.14.5, they seem to no longer work. I have verified that I can set the registers correctly, but they do not activate the associated start and stop functions.

Are you in Remote Mode?

yes of course, I have use it in many application

Is there a reason to need to run an outdated version of Polyscope like 5.14? They are on like 5.25 at this point. Maybe try updating that and see if your problem goes away?