Using this code to set a subtree as hidden and it doesnt appear to be working?
ProgramNodeFactory nf = programModel.getProgramNodeFactory();
FolderNode folderNode = nf.createFolderNode();
folderNode.setName(name);
folderNode.setSubtreeHidden(true);
return folderNode;
This is the error:
cannot find symbol
[ERROR] symbol: method setSubtreeHidden(boolean)
Any help would be greatly appreciated!
Are you using at least API version 1.12?
That’s a fairly new API (I think the current is 1.13) so if you’re using this on a slightly older build, it might not see it. You can find this in your POM under dependencies:
<dependency>
<groupId>com.ur.urcap</groupId>
<artifactId>api</artifactId>
<version>1.10.0</version>
<scope>provided</scope>
</dependency>
In this case, my CAP that is currently on 1.10 would also not be able to access this method.
1 Like
Amazing thank you! Was using the new API but hadnt changed the POM