SDK installation in staterkit

When I try to execute install.sh in starter kit with sdk 1.3.55 I have to input password.

But, I did not set up any password.

How can I know or input this password?

ur@urcapsstarterpackage:~/sdk/sdk-1.3.55$ ./install.sh
The tool ‘dialog’ is installed…
The tool ‘sshpass’ is installed…
The tool ‘mvn’ is installed…
Installing archetype and API to maven repository…
Installing older API versions to maven repository…
Installing additional jars…
Optional: Do you want to install the UR C/C++ cross-compiler toolchain? The toolchain minimally requires a x86_64 host system and Debian-based OS (y/N)?y
Installing native UR tool chain…
[sudo] password for ur:

I found it! Thank you

@anon74041429
What did you find our, and what was the answer?