Hi,
Exactly when are the installation variables saved to disk?
Is it possible to force the installation variables to be saved, when the robot is in “Run Program”?
Hi @anon62734967,
The installation variables are saved every ten minutes when running and during the controller shutdown process. I do not believe there is a way to force the installation variables to save more regularly, so if this is necessary I would recommend that instead of using the standard installation variables you use XMLRPC to pass your variables to a Python Daemon that then saves them to a text file on demand.
Thanks @ajp for the detailed answer.