Hi,
RTDE SETUP_INPUTS response is IN_USE for inputs when the Ethernet/IP is activated, even when no scanner are connected.
Tested with the last Virtual Machine 3.8.0.61336
Strange behaviours ?
Hi,
RTDE SETUP_INPUTS response is IN_USE for inputs when the Ethernet/IP is activated, even when no scanner are connected.
Tested with the last Virtual Machine 3.8.0.61336
Strange behaviours ?
Ethernet/IP and Profinet will reserve the following RTDE input blocks when activated (regardless of connection state).
Thus these signals will not be available for other clients, when Profinet or Ethernet/IP is activated.