So I’ve been getting this error every since I wrote this line of code (self.io = rtde_io.RTDEIOInterface(host)) in the init part:
RuntimeError: One of the RTDE input registers are already in use! Currently you must disable the EtherNet/IP adapter, PROFINET or any MODBUS unit configured on the robot. This might change in the future.
If I remove the line of code (self.io = rtde_io.RTDEIOInterface(host)), I do not get this error.
This is what I’ve tried to resolve this but haven’t been successful:
- All the Enternet, Prfinet and MODBUS endpoints are disabled.
- I tried SSHing into the robot to check active connections but I get the error
could not understand: 'netstat --all --program | grep 30004' - Restarting robot
Does anyone know what can be done to troubleshoot this error?