Hi All,
How to know the exact payload carrying capacity of the UR10e at a distance of supposedly 1000mm from the base. Is there any ratio in which this can be calculated. Payload to Reach ratio
Hi All,
How to know the exact payload carrying capacity of the UR10e at a distance of supposedly 1000mm from the base. Is there any ratio in which this can be calculated. Payload to Reach ratio
Hi @anon66049751, the new UR10e can carry 12.5kg across the whole robot workspace. If the center of gravity of the payload is offset significantly from the robot tool flange, cycle time may be automatically lowered by the robot controller, but full payload across full workspace is always maintained.
Just like our other robots, the COG Load curve will be provided in the User Manual. It has not been released yet.