Summary
I want to set lower speed value than 160 mm/s to Tool Speed in case of Reduced Mode.
What is it?
When I set a value to Tool Speed in case of Reduced Mode, minimum value is defined as 160 mm/s as below, so I can’t do it. For example, I wanna set 10 mm/s to it.
Why is it needed?
From a safety perspective, 160 mm/s is still considered a high speed, particularly when a UR robot handles sharp objects at its tool point.
(Even when operating in Reduced Mode, a sharp object impacting a person can result in injury.)