Hello, i am working with ur10 and i have a problem with the code size. The robot is connected via sockets with my pc and I send the code directly from here. When the route points are less than 500, the robot starts work smoothly, over 500 points the robot stays silent. It seems a memory problem …
can you send the queue in real time line by line? Or is there any special feature to be enabled because over 500 points do not give rise to problems?