Hello,
I’ve updated our URCap to work with the new PolyScope version 3.5.
In this version new values have been added to the real-time data stream of the UR robot (port 30003).
By consulting the the official specification (Remote Control Via TCP/IP - 16496)
I’ve noticed an error. According to the specification the new real-time message
consists of 1076 bytes, but this value is wrong. The correct value should be 1108. 6 double values have been added with 8 bytes each, so 48 bytes total.
=> PolyScope 3.4: 1060 bytes
=> PolyScope 3.5: 1108 bytes (+ 48 bytes/6 double values)
I hope this was the correct way to inform about the error.
Kind regards,
AM
Thank you for this report.
The bug have been reported.