Hi all,
I made a URCap using the ursim software. Now I’m trying to test the software on an actual UR but I am running into a problem. When I press on a textfield in PolyScope I am expecting the keyboard to show up so I can input a value but the keyboard doesn’t show up. Does anyone know how this can be fixed?
For example: When I press on the port to change this value. No keyboard shows up and I am not able to change anything. The ComboBox however does work fine.
Here’s an example of a double keyboard attached to a button:
You can get an instance of keyboardFactory through apiProvider.getUserInterfaceAPI().getUserInteraction(). I’ve just made a class containing all the different types so I don’t have to type it every time.
Here’s the getDoubleKeyboard() method:
You can do something similar just replace all the Doubles with Ints
Thank you, I have managed to solve my issue using the following implementation:
public KeyboardTextInput getKeyboardTextInput() {
return keyboardFactory.createStringKeyboardInput();
}
public KeyboardInputCallback<String> getKeyboardTextInputCallback() {
return new KeyboardInputCallback<String>() {
@Override
public void onOk(String tosettext) {
String field = getSelectedInputField();
if(field.equals("IP")) {
view.setIPTextField(tosettext);
}else if(field.equals("PORT")) {
view.setPORTTextField(tosettext);
}else if(field.equals("NAME")) {
view.setNAMETextField(tosettext);
}else if(field.equals("ATYPE")) {
view.setATYPETextField(tosettext);
}else if(field.equals("PMC_LOC")) {
view.setPMCLOCTextField(tosettext);
}else if(field.equals("BIT")) {
view.setBITTextField(tosettext);
}else if(field.equals("DTYPE")) {
view.setDTYPETextField(tosettext);
}else if(field.equals("PIN")) {
view.setPINTextField(tosettext);
}
}
};
}
This allows me to handle multiple textfields on the same page.