I need to run an URCAP similar to the example of the Ellipse.
However before adding the waypoints derived from the central point, I need to check if the POSE are reachable.
Is there any URCAP command for it or do I need to use some server communications such as port 30001?!?