[IMPLEMENTED] Adding variables

In the installation contribution part of your URCap you add and remove functions that can be used to assign variables during run time. Here is an example of how to add/remove functions to the function model. image

The functions will need to be within the generateScript(ScriptWriter writer) portion of the URCap installation contribution example: image

Adding the function to the function model would then be: image

Now within the program tree of the UR you can assign a variable from the function drop down menu example:


Sorry for long post but hope this helps you out!