Hey there,
I am using a UR5e with Polyscope 5.11. Is there a way to increase the voltage of the POWER-Pin of the tool connector? I would like to use a 48 V tool instead of the regular 24 V (or 12 V) tools.
I guess, using the Digital power output TO0/PWR and POWER in a row would not work? The manual only suggests “dual pin mode” using them in parallel.
And what is the maximum output current? In the manual it says max 2000 mA supply current, for single and even for dual pin mode. I am thinking of a step-up converter with the tool as a second solution, but this option would drag 3.5 A at the 24 V power output.
Third solution would be using a void pin from the tool connector an powering it up externally. But then the question would be which one to use. Because I also want to use a Robotiq 2-finger gripper and a Robotiq vacuum gripper interchangeable with the other tool, therse grippers should not suffer from the overpowerd pin. As far as I am seeing it, both grippers are only communicating on the analog pins (also called RS 485 pins).
This would mean, that I can use any of the digital I/O pins for the higher voltage powering.
Cheers,
Thomas