(This post is a Wiki, experienced developers can modify the content)
This post describes the electrical interfaces of a Universal Robot, UR3, UR5 or UR10.
There are electrical interfaces (analog and digital) in the controlbox and at an M8 connector at the tool.
Control box
16 digital inputs (0/24V DC)
16 digital outputs (0/24V DC)
2 analog inputs (0-10V DC or 4-20 mA, 12 bit, differential)
2 analog outputs (0-10V DC or 4-20 mA, 12 bit, differential)
The internal 24V PSU can supply a maximum current of 2A total. An external 24V PSU can optionally be used to increase power.
Any digital input can be configured in PolyScope software or via the URScript interface, to have a functionality to be an external Play, Pause, Stop or Freedrive button.
@anon28291296,
The constant current drain of the tool is 600 mA.
A peak above this should be no longer than 1 ms.
The actual peak current capability is not rated.
Any digital input other than the configurable inputs can be configured to by a play/pause/stop/freedrive input. It would be nice if those could be configured as well
I cannot see a way to set configurable inputs to these functions like I can standard and tool inputs. Here is a screenshot of a standard digital input where it shows the IO Action dropdown menu
@jbm is not clear to me from both this post and the UR5 manual whether the max current drain of the tool (600mA) is related only to the internal power supply (which provides a global upper limit of 2A), or it is a strict limitation even if an external power supply is connected to the system, which raises the the maximum absorption up to 6A.
As you can imagine, our end-effector requires more than 600mA.
The combined max. current draw from the Tool connector is 600 mA.
The 12 V or 24 V power at the tool is generated locally on the Tool, and has nothing to do with the power in the Control box. Hence an external PSU does not change this limit.
In the controlbox there is an internal PSU with a cap of 2 A total, combined for all 24 V terminals and outputs.
You can skip this PSU, and use an external 24 V supply as specified in the User Manual, where the max. allowed current through the control box terminals is 6 A.
Thank you for the quick reply. I had a look at the link you sent me. Is it possible to get a more detailed description of the internal structure of the Tool_Mounting_Bracket that appears on page 5 of UR3_schmatic_drawings_rev3.0.3.1.pdf?