How can i base a point on a plan?

I would like to base a point on a plane, and as that plane moves, the point changes as well.

These are called ā€œFeaturesā€ in Polyscope and you can find them in the Installation Tab. You can teach a plane, and then moves can select this Feature.

image

Just be sure to select the feature BEFORE setting the Waypoint, as changing the feature after the point is set will result in a bad time.

Yes, I know that. but I would like to do this in the script, as I will change the plan every cycle, and the only way I have found to create a plan every time is within a script.

You can change the plan programmatically via script by just calling pose_add() or pose_trans() and pass in the feature and however you want to transform it. So for example if every cycle you need your point to shift along the X-axis 100mm, you’d do:

image

If it helps, there’s nothing special about a Feature. Polyscope just sees it as a pose. So in that guy’s example you linked to, he could just write a seeking script using the force function, and record each offset and pass THOSE into the pose_add()/pose_trans() functions.

Not sure what specifically you’re looking for here. Teaching a point to a feature solves your original question, and this allows it to change the offset per cycle.