Hi All,
Im trying to offset a defined waypoint thought w.r.t a feature plane. We would have normally done this by setting the plane as a variable and moving the plane in the x/y direction required.
With the newer version of Polyscope, this variable plane feature is not an option any more.
How can I realize this with the functionality available.
Thanks
Taught features are variable by default now.
If you have a plane feature, Plane_1, and add an assignment node or open the variable drop-down, you’ll see Plane_1 listed there. You can then edit as normal.
The actual position of the feature is available as a pose, Plane_1_const, if you needed access to the coordinates of the feature relative to the base frame.
Thanks for that info. But I’m still unclear how I add an offset to a way point and get it to move in the plane.
Do I do a trans pose on plane and offset, then moveL plane, way point?
You move the feature (variable) by assigning it a new value. p[x,y,z,rx,ry,rz]. The waypoints in a move that has this feature selected will move with the feature
Check out the e-Learning for more details.
https://academy.universal-robots.com/free-e-learning/e-series-e-learning/e-series-pro-track/