Hi guys,
I have a lot of installation variables that various programs use. I have a select few which are favorites that the operator will only see when running the program.
There is one variable that the operators need to adjust every now and then via the installation variables page.
Is there any way to hide the other variables so that only the variables that the operators adjust will be visible and the operators can’t accidentally change the wrong ones?
So far we are only using the pendant
Thanks in advanced for any tips
There’s no way to hide select variables in the Installation tab. My best suggestion would be to prompt the operator every time the program starts, asking if they want to change this specific variable, using the Assignment node and then choosing Operator Input in the top right corner.