This is my code to get all the variables on my instalaltion but I cannot find methods to get the value of the variable. The objective is to visualize some variables (such as counters) in a toolbar.
import java.util.Collection;
import java.util.Iterator;
import com.ur.urcap.api.domain.variable.Variable;
import com.ur.urcap.api.domain.variable.VariableModel;
public class VariableHandler {
private final VariableModel variableModel;
public VariableHandler(VariableModel variableModel) {
this.variableModel = variableModel;
}
/*Returns variable object found by its default name
*
*/
public Variable getVariable(String defaultName){
Collection<Variable> Variablecollection = variableModel.getAll();
int VAR_count = Variablecollection.size();
if(VAR_count > 0){
Iterator<Variable> VAR_itr = Variablecollection.iterator();
while(VAR_itr.hasNext()){
Variable thisVAR = VAR_itr.next();
String thisDefaultName = thisVAR.getDisplayName();
System.out.println("Found A VAR named "+thisDefaultName);
if(thisDefaultName.equals(defaultName)){
return thisVAR;
}
}
}
return null;
}
}
Thanks.
This is not as simple. I’m also trying to find the best way to view and edit a variable from a toolbar. These are the possibilities I know to get the current value of a URScript variabile in a URCap:
- Read it from Primary Interface - You have to write a “reader” for the packages sent by the controller, maybe based on this sample which is for Realtime: getRobotData
- Send it from URScript through a socket to a java server (see ScriptCommunicator or this older one ScriptCommunicator)
- Send it from URScript through XML-RPC (see
mydaemonswing sample or Dialog Script URCap)
I think maybe the second method is the simplest one.
I tried with the ScriptCommunicator (the ScriptExtractor part), but I can get only data by using built-in function like get_…().Do you have an example where you get the value of a pose (like i_home_pose) or a general int variable (i_var_1) stored in the installation variables?
You are correct, I forgot I was using scriptExporter to export a value from the integer registers, as e.g.:
ScriptExporter export = new ScriptExporter();
ScriptCommand commandInt = new ScriptCommand("Command1");
commandInt.appendLine("int_value = read_output_integer_register(21)");
int resultInt = export.exportIntegerFromURScript(commandInt, "int_value");
So a possible workaround is to constantly copy the variable you are interested in to a register and read from that. Sorry but I don’t know if it is possible to read a variable with this code.
Thank you!!! I did not know this feature, I’m testing it right now and it’s working. It is a good workaround.