Ethernet IP Scanner / Profinet Master

Hi there,
are there some plans from UR to use the Robot Controller as Ethernet IP-Scanner or Profinet-Master?
Greetings

I would second this as a feature request!

I would like to have the UR as a Profinet master (IO Controller).

I would also like UR to support ProfiSafe over Profinet. ProfiSafe would eliminate a lot of discrete wiring with our installations.

I would also like to see ProfiSafe.

Profinet Master would also be appreciated here. :point_up:

+1 on the EIP scanner request

EIP Scanner, Profinet Master Please

Also update Modbus to use all Function codes and double word