Software version: 3.12
Robot generation: CB31 UR5
Steps to reproduce:
- First step: start the robot
Expected behavior: normal boot
Actual behavior: error message while loading polyscope
Hello everbody,
I´ve just updated my UR5 CB31 to SW Version 3.12.0, previous version was 3.11.0. As you can see in the attached picture, I got an error message without any notes while loading polyscope. The message appears at 21% and stays until 100%. If I don´t touched the “OK Button”, the systems stucks at 100%. Only after clicking three times the “OK Button”, it forwarded me to the normal menu.
Beside this error, I didn´t found any others failures until now. I allready uninstalled all UR Caps, but it didn´t change the behaviour.
Even if there is no other error, I want to know the reason and optimally solve the problem with the error message.
Do you have any tips for me?
Many thanks in advance and best regards,
Frederik