Hello everyone,
in our Application we want to secure our robot by using multiple safety ground scanners and connect them directly to the robot using their OSSD-Outputs. However if I try to assign multiple inputs in Poliscope as “Automatic Mode Safeguard Stop” it always sets one of them back to “Unassigned”. Is it possible to Assign multiple inputs to the same function? If so, how would I do that?
@terryc I know that i could realize it that way or with a safety PLC but i wanted to know if it would be possible to assign multiple inputs to this function as it would eliminate the need for a relatively expensive safety PLC.
I also took al look if it would be possible to modify the installation file in a way that makes this possible but unfortunately in the installation file the I/O numbers are assigned to the functions not the other way around which makes this impossible.
If i didn’t overlook a way of doing this please see this as a feature request as it would help cut down costs for integrators.