Does anyone know how to set up the dashboard server with an M340 PLC from Schneider. I was told that it is not possible to set up a different port number , in this case 29999, than the ones set up according to the differents networks. Thank you
I had the information, apparently with the Schneider M340 all the ports are established acording to the type of connections, we cannot change it.
So I will use another PLC as an interface (a small one) a M241 in which we can set the ports by programming a socket (IP address, port).